Technical FAQs

Ask a Question

Do the open style Altivar 58 drives have internal fuses?

It depends on the size of the drive.
All of the 230 VAC drives do not have internal fuses.
All of the 460 VAC drives up to the D79N4 size do not have internal fuses.
All of the 460 VAC drives from the C10N4 and larger do have internal fuses.
If internal fuses are suspected of damage, please contact Drive Products Support at 888-SQUARED (888-778-2733) for technical assistance.


CTA-ID : 4405
Was this helpful?
What can we do to improve the information ?