Technical FAQs

Ask a Question

How does the two color illuminated selector switch , 9001K, 9001KX or 9001SK, work?

Issue:
How does the two color illuminated selector switch , 9001K, 9001KX or 9001SK, work?

Product Line:
30mm Push Buttons

Environment:
9001 Type K/ SK/ KX Selector Switch

Cause:
Explanation of how the light module changes colors.                       

Resolution:                                                                 
There is a 2 color red and green film behind a clear knob. When knob is turn to left lamp illuminates through red side and when turned to the right it illuminates through the green side.
 
Was this helpful?
What can we do to improve the information ?