Technical FAQs

Ask a Question

How many degrees of travel are there from position to position for the 9001SKS11 selector switch?

The angle between positions is 70 degrees or 35 degrees each side of 0 degrees.
Was this helpful?
What can we do to improve the information ?