Technical FAQs

Ask a Question

Can a HOM30L150C, Series S1 load center be converted to a main breaker load center?

Yes. A QOM2-VH, Main Breaker Kit (150A maximum) can be field installed. For a 150 A application, use QOM2150VH.

CTA-ID : 2026792
Was this helpful?
What can we do to improve the information ?