Technical FAQs

Ask a Question

Can AI3 be used as the PI feedback if an I-O extension is used?

Yes. If using 0-10 VDC signal jumper AI3B to COM since AI3 is a Bi-polar input.

Actual functionality of the PI control depends on the revision level of the drive in use.
See the keypad programming manual for details.


CTA-ID : 2013337
Was this helpful?
What can we do to improve the information ?