Technical FAQs

Ask a Question

Does the RC200S, RC2M200S or RC2M200SH Combination Service Entrance Devices, come with a bypass provided on the meter socket?

Issue:
Product design

Product Line:
Combination Service Entrance Devices

Environment:
Meter socket feature

Cause:
Applicaiton

Resolution:
A bypass is NOT provided on the RC200S and RC2M200S, but the RC2M200SH is provided with a Horn Bypass factory installed.
 
NOTE: The RC2M200SH and RC2M200S will both accept a second main service disconnect(or main breaker), a QO-VH type, up to 50Amp maximum for Field Installation.





CTA-ID : 2026690
Was this helpful?
What can we do to improve the information ?