Technical FAQs

Ask a Question

Is there a way to prevent the Altivar 58 drive from being controlled by the serial communications?

Yes. An input can be assigned to forced local. When this input is high the drive will ignore serial commands.
Also, the freewheel stop and fast stop commands override serial communications.


CTA-ID : 6805
Was this helpful?
What can we do to improve the information ?