Technical FAQs

Ask a Question

Can a Neutral be field installed in a HU265?<br /><br />

A H600SN (or an H600SNC for copper wire only ) can be field installed in this device.


CTA-ID : 2026994
Was this helpful?
What can we do to improve the information ?