Technical FAQs

Ask a Question

Can PI control be used when the Altivar 58 drive is controlled by Serial Communications?

Yes.  If the drive is set up for PI over Serial com it uses the AI2 as a feedback signal. The drive can receive the start/stop and setpoint commands via Serial Communications.

Also, most PLCs can perform the PI internally and control the drive directly.

CTA-ID : 2010169
Was this helpful?
What can we do to improve the information ?