Technical FAQs

Ask a Question

Is the value of the Altivar 58 PI Presets in actual hertz or a percentage of signal?

The value of the PI presets is in percentage not hertz. The PI presets are setpoints for the PI control. The PI control will try to adjust output frequency with the objective of making the feedback signal equal to the setpoint.

Actual functionality of the PI control depends on the revision level of the drive in use.
See the keypad programming manual for details.

CTA-ID : 2008702
Was this helpful?
What can we do to improve the information ?