Technical FAQs

Ask a Question

Why does the August 2001 keypad manual not show anything regarding setting up the ATV58 for use with preset setpoints with PI operation?

At the time the manual was published the drive did not have this feature available.
The operation for PI preset inputs did not occur in unit until the version 4.1 firmware upgrade. This was in Late 2001.

Actual functionality of the PI control depends on the revision level of the drive in use.
See the keypad programming manual for details.


CTA-ID : 2008700
Was this helpful?
What can we do to improve the information ?