Technical FAQs

Ask a Question

What are the repair parts for the H362WC, series F6 (may be shown as F06)?

The repair parts for the H362WC, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly -40566-038-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-040-50 (requires one per switch)
Line and Load Base Mounting Screw - 40205-151-01(3 for line & 2 for load)
Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
Arc Suppressor Mounting Screw - 40205-145-01
Mechanism Assembly - 4056787350 (NOTE: also recommend replacing Handle Gasket)
Mechanism Washer - 2360200008
Handle Assembly - 4056663550 (also recommend replacing Handle Gasket)
Handle Gasket - 4056603101
Lockplate - 4056672101
Lockplate Mounting Screw - 2299940562 (2 required)
Rod/Linkage Assembly - 4056787050
Lug Kit - AL0306F (one kit includes all line and load lugs)
Receptacle - 25410-023-11
Receptacle Mounting Screws - 45102-801-01 (required 4)



CTA-ID : 2026240
Was this helpful?
What can we do to improve the information ?