Technical FAQs

Ask a Question

What is the number for the screws that hold the starter in the enclosure of Well Guard pump panel 8940SSC4010?

21911-14103 is the screw number, 8/32`` x 5/16``, three are required.


CTA-ID : 2026680
Was this helpful?
What can we do to improve the information ?