Technical FAQs

Ask a Question

What size speed pot is recommended for the Altivar ATV66?

It will work with any potentiometer with a rating from 1k Ohms to 10k Ohms.
Could use ATVPOT25K. It is a 22 mm operator with a pot that is 2,500 ohms.

CTA-ID : 6946
Was this helpful?
What can we do to improve the information ?