Technical FAQs

Ask a Question

What is the suggested value of the speed potentiometer for the Altivar ATV16?

It will work with any potentiometer with a rating from 1k Ohms to 10k Ohms.
Could use ATVPOT25K. It is a 22 mm operator with a pot that is 2,500 ohms.


CTA-ID : 4248
Was this helpful?
What can we do to improve the information ?