Technical FAQs

Ask a Question

Can the main breaker in a QO342MQ150 or QO342MQ200 be upgraded to a higher ampere rated main breaker?

Issue:
Application

Product Line:
QO Load Center

Cause:
Application

Resolution:
The labeling on these load center state: MAIN 225A MAX.
To upgrade the 150A load center to 200A order QDL32200; to 225A order QDL32225.
To upgrade the 200A load center to 225A order QDL32225.

CTA-ID : 2026982
Was this helpful?
What can we do to improve the information ?