Technical FAQs

Ask a Question

What cables do I use to connect my TWIDO PLC using TWDDDO16DK (output module) and TWDDDI16TK (input module) and LU9G02 (splitter) to connect to U-Line controllers with LUFC00 (parallel connector function module)?

For the TWDDDO16DK output card use ABFTE20SP*00 where the * is either 1, 2, or 3 for cables of 1 meter, 2 meter and 3 meter length, respectively.

For the TWDDDI16TK input card use ABTFE20EP*00 where the * is either 1, 2, or 3 for cables of 1, 2 and 3 meter length, respectively.

The cables listed above have HE10 20 way connectors on each end.

The cable (with RJ45 connectors on each end) between the splitter and the parallel function module on the U-Line is VW3A8306R** where the ** is 03, 10 or 30 for cable lengths of 0.3, 1, and 3 meters, respectively.

NOTE: DO NOT USE the TSXCDP*** cable with TWIDO modules. Use of this cable will damage the TWIDO input and output modules. The pin configuration is different for the TWIDO modules when compared to other PLCs (such as Quantum and Premium).



CTA-ID : 2026669
Was this helpful?
What can we do to improve the information ?