Technical FAQs

Ask a Question

Does the Altivar 58 drive have Sensorless Vector Control?

Yes. The Altivar 58 is a sensorless flux vector control type drive. The settings and options used with the drive can be changed to allow increased or decreased control.
Note: There are Altivar FVC drives that are Flux Vector Control drives that can use encoder feedback. Also, on the standard drive it is possible to add the digital I-O extension card (VW3A58202U) to allow encoder feedback.


CTA-ID : 6894
Was this helpful?
What can we do to improve the information ?