Technical FAQs

Ask a Question

It is possible to use +/- speed control and reference switching with an Altivar 58 drive?

No. These two functions are not compatible and can not be programmed into the same drive at the same time.
See the keypad programming guide for additional information about these and other functions.

CTA-ID : 6892
Was this helpful?
What can we do to improve the information ?