Technical FAQs

Ask a Question

Can the Altivar 28 be set up for 2-wire control in Level detect (LEL) mode similar to Altivar 31?

The Altivar 28 is an obsolete drive.
With factory settings for 2-wire control the drive needs to see a transition on the run command.
At power-up the forward or reverse input must transition from low to high before the drive will start the.
This can be changed by setting Atr (Auto Reset) in the DRC menu to yes. This works like LEL in the Altivar 31.
The ATV28 drives do not have a tCt code (trn or lel), factory default works like trn.
See the manual for additional details.


CTA-ID : 2027055
Was this helpful?
What can we do to improve the information ?