Technical FAQs

Ask a Question

Is the small load center QO24L70RB rated for 22K AIC?

No. That small enclosure is rated at only 10K AIC. It cannot utilize the higher AIC breakers such as the QO-VH 22K AIC type .

CTA-ID : 2026972
Was this helpful?
What can we do to improve the information ?