Technical FAQs

Ask a Question

Does Square D offer 400Hz rated 9070 control power transformers?

Issue:
Does Square D offer 400Hz rated 9070 control power transformers?

Product Line:
Dry type low voltage transformers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Square D does not offer 400Hz rated control power transformers as part of the standard basket of products. However, Square D can build them if the OEM opportunity is attractive. Contact your local Field Office if an OEM opportunity arises.


CTA-ID : 2026971
Was this helpful?
What can we do to improve the information ?