Technical FAQs

Ask a Question

Is the load center QO142L225G rated at 22K AIC?

Depending on the circuit breakers you install, that load center is rated up to 65K AIC. The Load center assumes the rating of the circuit breaker that has the lowest AIC rating.


CTA-ID : 2026969
Was this helpful?
What can we do to improve the information ?