Technical FAQs

Ask a Question

Is it possible to remove the main breaker from a QO120M100, and install it in QO132L125G load center?

Yes. Both panels accept the QOM1 frame breaker.


CTA-ID : 2026785
Was this helpful?
What can we do to improve the information ?