Technical FAQs

Ask a Question

Need replacement module for a TVS4EMA32A

2 each per phase modules part # MA4IMA16. Not both modules need to be replaced at once, only the module that is not operational. Each module has 2 green LEDs lit if modules is operational. If only one LED is lit, or no LED`s are lit on the module,then it requires replacement.

CTA-ID : 2026783
Was this helpful?
What can we do to improve the information ?