Technical FAQs

Ask a Question

How can external contacts be used to stop the Altivar 58?

There are multiple ways to stop the ATV58 drive. The stop method used depends on how the drive is being controlled. It is very important to configure the controls correctly.
The most common control method is 2-wire control. To run, a connection is made from +24 to LI1 for forward or LI2 for reverse. Remove the forward or reverse run command to stop the drive.
Another common stop method is to program one of the Logic inputs (LI2 - LI6) for freewheel stop (nSt) or fast stop (FSt). When this input is de-energized the drive will stop regardless of the method used to run the drive.
For other ways to stop the drive from running see the keypad programming manual.


CTA-ID : 6816
Was this helpful?
What can we do to improve the information ?