Technical FAQs

Ask a Question

How can the configuration settings be stored in the keypad for an Altivar 58?

Make sure the keypad is not locked and the drive is not running.
Go to menu 7 (Files menu). Enter
Go to Operation Type (FOt). Enter
Go to Store File (Str). Enter
Select a file number 1-4. (The keypad can store up to 4 different configurations.)
Enter. Enter again to verify.
The display will return to FOt when done.
See keypad programming manual for additional details.



CTA-ID : 2026910
Was this helpful?
What can we do to improve the information ?