Technical FAQs

Ask a Question

On a QOB1201021 breaker with a 120V shunt trip, there is a sticker that says on the side of the shunt trip, ``open when off.`` Should this circuit be open when the breaker is on?

The reference makes a distinction between the breaker state and the coil and clearing contact state. When the breaker is ``on``, the coil circuit is closed and waiting for a 120V signal to trip the breaker.

CTA-ID : 2026772
Was this helpful?
What can we do to improve the information ?