Technical FAQs

Ask a Question

Is a 82344NRB UL Listed?<br />

No. When the factory installed neutral is added, the switch then becomes non-UL device.


CTA-ID : 2026770
Was this helpful?
What can we do to improve the information ?