Technical FAQs

Ask a Question

What are the dimensions for new 600A Double Throw switches as of March 2006?

Cat. #.................H...............W...................D

DTU326............63.31........23.66..............8.88
DTU426............63.31........27.00..............8.88
DTU366............63.31........23.66..............8.88
DTU466............63.31........27.00..............8.88
DTU326R.........63.76........23.66..............8.88
DTU426R.........63.76........27.00..............8.88
DTU366R.........63.76........23.66..............8.88
DTU466R.........63.76........27.00..............8.88
DTU366AWK...63.76........23.66..............8.88



CTA-ID : 2026646
Was this helpful?
What can we do to improve the information ?