Technical FAQs

Ask a Question

What are the dimensions for new 400A Double Throw switches as of March 2006?

Cat #..................H........................W......................D

82255...............38.50.................26.10................10.63
82255R............39.00.................26.62................10.63
82345...............38.50.................26.10................10.63
82345DS..........39.00.................26.62...............10.63
82345R.............39.00.................26.62...............10.63
82355................38.50.................26.10...............10.63
82355R.............39.00.................26.62...............10.63
82445................38.50.................30.10...............10.63
82445R.............39.00.................30.21...............10.63
82455................38.50.................30.10...............10.63
82455R.............39.00.................30.21...............10.63
H82255.............39.00.................26.62...............10.63
H82345.............39.00.................26.62...............10.63
H82355.............39.00.................26.62...............10.63
H82445.............39.00.................30.21...............10.63
H82455.............39.00.................30.21...............10.63



CTA-ID : 2026645
Was this helpful?
What can we do to improve the information ?