Technical FAQs

Ask a Question

What is the ring-tongue terminal required for the UL 489 Multi 9 C60 miniature circuit breakers with 480Y/277 Vac ratings?

Use single Thomas & Betts Cat. No. RD8-10 or equivalent UL listed and/or CSA certified insulated ring terminal only.
The max outside diameter is .45 in (11.5mm). Internal diameter for M5 screw (5mm).


CTA-ID : 2027073
Was this helpful?
What can we do to improve the information ?