Technical FAQs

Ask a Question

On an EZM tap box catalog number EZM1225TB, why is the neutral not bonded to the enclosure?

The EZM1225TB is supplied with an isolated neutral, and was designed as an output device only. Our smallest tap box with neutral-bonding capability is the 400A EZM1400TB, which is suitable for use both an input or output device.

CTA-ID : 2027071
Was this helpful?
What can we do to improve the information ?