Technical FAQs

Ask a Question

What voltages can be applied to the 1082 shunt trip on the EH/EHB breaker?

120 Vac, 208 Vac, 240 Vac or 277 Vac can be applied to this shunt trip.


CTA-ID : 2026950
Was this helpful?
What can we do to improve the information ?