Technical FAQs

Ask a Question

Do you need to order a coupling in order to put 2 sections of RSV092100120 together?

No. There is a small coupler device, which is called a `key`, on the rails that ties to rails together.


CTA-ID : 2026942
Was this helpful?
What can we do to improve the information ?