Technical FAQs

Ask a Question

Is an external motor overload relay required when the Output Phase Fault is disabled on the Altivar ATV66?

Yes it is recommended to use an external motor overload relay.


CTA-ID : 6720
Was this helpful?
What can we do to improve the information ?