Technical FAQs

Ask a Question

Is a retaining kit available to backfeed a HOM816M150FTRB or HOM816M200FTRB.


Product Line:
Homeline Load Center


Yes. As marked on the wiring diagram, the retaining kits are HOM4RK2HA and HOM5RK. The HOM4RK2HA will be used to retain back fed branch breakers rated through and including 125A. The HOM5RK will be used to retain branch breakers rated 150A - 200A. The retaining kit does not interlock the back-fed branch breaker with the QOM2200VH factory installed main breaker. For an application requiring interlocking a 125A maximum back fed branch circuit breaker to the factory installed main breaker, use HOMRBGK2 or HOMRBGK2C. 

CTA-ID : 2026644
Was this helpful?
What can we do to improve the information ?