Technical FAQs

Ask a Question

Can a Back Fed Main Circuit Breaker be field installed on a QON12L100, OEM Mounting Base?

Our Old QON12L100, OEM Mounting base is not built on a ``Convertible Interior`` and can not be used with a back-feed main configuration, because there was no retaining kit available to attach the Back-feed main circuit breaker to the rail of the QON12L100, OEM Mounting Base Interior.

CTA-ID : 2026636
Was this helpful?
What can we do to improve the information ?