Technical FAQs

Ask a Question

What was the AIR rating of the NHL breaker?

The NHL breaker was rated 50K AIR @ 480V, and 100K AIR @ 240V. It had no 600V rating.
Steve Flock / CR


CTA-ID : 2027054
Was this helpful?
What can we do to improve the information ?