Technical FAQs

Ask a Question

What is the difference between the 2510 MCR and the 2510MCT?

The 2510MCR NEMA 7 & 9 enclosures are cast iron. NEMA 4X, 7 & 9 cast aluminum enclosures are available for outdoor use. To order the NEMA 4X, 7 & 9 enclosed device replace the ``R`` in the part number with ``T``. For example 2510MCR3 becomes 2510MCT3.

CTA-ID : 2026930
Was this helpful?
What can we do to improve the information ?