Technical FAQs

Ask a Question

Do any EZM branch devices have a removable drip hood that covers the top endwall?

Yes, some of them include the removable drip hood. The devices that include this feature are all EZM branch devices that have a maximum tenant breaker rating of 125A (example catalog numbers EZM113125, EZMR113125, EZMH113125). Also, EZML branch devices with a ``D`` suffix on the catalog number include the removable drip hood (example EZML113225D). NOTE: remove the drip hood in INDOOR installations only.

CTA-ID : 2026750
Was this helpful?
What can we do to improve the information ?