Technical FAQs

Ask a Question

What are the dimensions of the SDM36BW Multi-Link Enclosure?

Issue:
Dimensions

Product Line:
Multi-Link

Cause:
Dimensions

Resolution:
The SDM36BW is 36.00" H x 14.24" W x 3.57" D.
Click this link for access to Approval Drawing #3208:
http://static.schneider-electric.us/docs/Electrical%20Distribution/Structured%20Wiring%20System/Multi-link%20Structured%20Wiring%20Systems/3208.pdf
The approval drawing is also attached for your reference.
NOTE: The Multi-Link product line is no longer offered, nor supported, by Square D Company


CTA-ID : 2026751
Was this helpful?
What can we do to improve the information ?