Technical FAQs

Ask a Question

What is the amperage/voltage ratings of the Powerbus 225 busway?

Issue:
What is the available amperage/voltage ratings of Powerbus busway?

Product Line:
Nema busway sold and supported in the USA.

Environment:
Selection/Specification

Cause:
Application

Resolution:
100A @ 600V AC maximum
225A @ 600V AC maximum
400A @ 600V AC maximum

.



CTA-ID : 2026622
Was this helpful?
What can we do to improve the information ?