Technical FAQs

Ask a Question

What functions can be assigned to the analog output on an Altivar 58 drive?

Motor current (OCr)
Motor frequency (OFr)
Output ramp (OrP)
Motor torque (trq)
Signed Torque (Stq)
Signed Ramp (OrS)
PI Reference (OPS)
PI Feedback (OPF)
PI Error (OPE)
PI Integral (OPI)
Motor Power (OPr)
Motor Thermal (tHr)
Drive Thermal (tHd)
Some of the functions listed were not available on older revisions of drive firmware. See the programming manual or option card manual (if used) for additional details.

CTA-ID : 6880
Was this helpful?
What can we do to improve the information ?