Technical FAQs

Ask a Question

Can the Altivar 58 drives be used with single phase input voltage and three phase output to the motor?

Yes. The 208 / 230 VAC ATV58 drives have been tested for single phase input.
The ATV58HU72M2 and larger require a 3% line reactor to be used for single phase input applications. Input phase loss fault must be disabled. Please pay attention to proper size selection.

See the installation guide for more details.

CTA-ID : 6875
Was this helpful?
What can we do to improve the information ?