Technical FAQs

Ask a Question

Can the analog output of the Altivar 58 be adjusted to range other than 0 to 20 mA?

Yes. The Control menu allows the low (CrL) and high (CrH) ranges to be changed.

See the keypad programming manual or option card manual (if used) for more details.

CTA-ID : 6868
Was this helpful?
What can we do to improve the information ?