Technical FAQs

Ask a Question

What is the adjustable width of the plungers on the Class 9066 Type RA2 or Type RA3 external reset mechanisms?

From 2 to 7 inches in 1/2 inch increments.


CTA-ID : 2026924
Was this helpful?
What can we do to improve the information ?