Technical FAQs

Ask a Question

Are the Powerpact H and J frame UVR devices ``kiss-free?``

The Powerpact H and J frames do have kiss-free UVR devices. This means if the UVR has no power, operation of circuit breaker closing mechanism will not permit the main contacts to touch, even momentarily.


CTA-ID : 2026919
Was this helpful?
What can we do to improve the information ?