Technical FAQs

Ask a Question

On circuit breaker catalog number MAL368002249. What does the suffix 2249 stand for ?<br />

The 2249 suffix is a combination of two factory installed devices on the breaker. The first is a 1212 1A/1B auxiliary switch, and the second is a 2103 normally closed bell alarm switch.


CTA-ID : 2026739
Was this helpful?
What can we do to improve the information ?