Technical FAQs

Ask a Question

Where do the control wires go when I wire to the shunt trip accessory on a PowerPact J frame lug to lug breaker? There is a cover on the front of the breaker that has no holes in it.

The wires can be routed through knockouts which are scored on the inside top of the front accessory cover, per the instruction bulletin that comes with the breaker.


CTA-ID : 2026735
Was this helpful?
What can we do to improve the information ?